2008-11-28 01:42 AM
2011-05-17 12:56 AM
Hi all, as a student getting started to learn embedded (Linux) system, I'm looking for a nice development board, which embodies a 32bit ARM9 processor and some useful connection (USB, 2 or 3 serial, ethernet, camera...). For me as a beginner, I need it to be ready to run and inexpensive (<=$300), pre-configured tool chain and necessary binaries, example projects included.
better would it be if it has been attached with a LCD Thanks in advance for any information that would be helpful.2011-05-17 12:56 AM
You may would like to check the
from ARM920T CPU 64M SDRAM+64M NAND FLASH+2M Nor Flash USB HOST and device 3 serial ports SD card slot 3.5'' TFT LCD ... Price=€200= about $251 seems a great board, I have bought it 2 days ago and will get it soon :) :D2011-05-17 12:56 AM
hi,
I m not an expert about embedded linux, but seems need a external memory controler, with ''huge'' quantity (in comparaison to the STR9 embedded 96K of RAM). Same idea with flash. Take a look with Atmel, they make some ARM9 at 180-200 Mhz (i forget the name of these device), really well supported by linux and the community and with plenty of documentation as / how tu use GCC, linux... Good luck.