2007-10-17 05:14 AM
ST7LITE15BF0, option bytes and InDART-STX ?
2007-10-17 05:14 AM
Hi,
I have developped a first application with the ST7LITE15BF0 and it works fine! Just a last problem : When I connect my target board to my InDART-STX debugger, if I use the option bytes it doesn't works (dial stopped between InDART and my board). If I don't use option bytes and use the InDART clock applyed on pin 20 of the controller, it works. So I can debbug an then I program the FLASH and the option bytes, I deconnect the InDART and it works? With old cards with ST7LITE05, I can debbug with the option bytes programmed using the internal RC as oscillator when the InDART is connected? What are the diferences and why this behaviour differences between the 2 micro's? Is there any possibility to debbug a ST7LITE15BF0 with InDART using the micro internal RC? Thank you to give me an answer. Regards Whitebull