2005-04-12 11:19 PM
2005-04-07 12:21 PM
no need
and why u use a OSC in MCU Then ?? u must send data and do some Delay() using Internal Osc (count the Cycles) and the Receiver will Read and wait the same Delay2005-04-12 11:19 PM
Guys,
Thanks for your responses. But I am still not clear on how to connect to PIC.I have read through Developpment Kits. I have various periferals on PIC already Programmed I only need to ADD PLM. So just adding 3 wire is it enough or do I have to uses some more wires. Please can any one tell me what is the range of ST7538. Can it be used gor Industrial purpose.