cancel
Showing results for 
Search instead for 
Did you mean: 

SPI bus speed

julienduay
Associate II
Posted on January 08, 2007 at 00:19

SPI bus speed

6 REPLIES 6
julienduay
Associate II
Posted on March 08, 2006 at 10:49

Hello,

I want to transfer data with a MMC card.

What is the maximum speed in Mhz of SPI bus on STR710 chip?

Thank you

:-)

julienduay
Associate II
Posted on March 08, 2006 at 11:17

I want to know the maximum BSPI bus speed in master mode (in Mhz).

Thanks

hichem2
Associate II
Posted on March 08, 2006 at 11:44

Hi,

Each of the two SPIs allow full duplex, synchronous communications with external devices,

master or slave communication at up to 5.5Mb/s in Master mode and 4 Mb/s in Slave mode.

Hich :-P

julienduay
Associate II
Posted on March 08, 2006 at 11:58

Thank you very much, but I want to know the max speed of BSPI bus in Mhz.

-> APB1 /6 in master mode = X Mhz ?

jorge2399
Associate II
Posted on January 05, 2007 at 11:57

Quote:

On 08-03-2006 at 16:14, Anonymous wrote:

Hi,

Each of the two SPIs allow full duplex, synchronous communications with external devices,

master or slave communication at up to 5.5Mb/s in Master mode and 4 Mb/s in Slave mode.

Hich :-P

I would to have a little precision : is 4 Mb/s the maximum speed in Slave mode? Is'n it 4.096MHz ?

Thanks for reply,

Regards,

javidaboo
Associate II
Posted on January 08, 2007 at 00:19

It looks like 4.096 mhz is the clock frequency. Did I say the clock frequency. The STR should be running at a higher speed using the PPL. Read the manual on the OSC, PPL and SPI.