Skip to main content
daniel8
Associate III
December 10, 2009
Question

Remapping interrupts

  • December 10, 2009
  • 2 replies
  • 878 views
Posted on December 10, 2009 at 18:36

Remapping interrupts

This topic has been closed for replies.

2 replies

tomas23
Visitor II
May 17, 2011
Posted on May 17, 2011 at 09:59

You have to dig into assembly :)

Check attached files, beware of start-up codes and changes in linker files, they are CRITICAL to proper IVT forward.

Modify according to your needs.

daniel8
daniel8Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:59

I am trying to implement the fix for Rev. G silicon where I do not remap the FMI to jump to Bank0 , and instead just jump to 0x80000 to execute the code. The problem is the interrupts do not remap, and I cannot figure out how remap them. If I set in Bank1 the irq_handler address to bank 0, the interrupts work, but then of course the interrupts do not work in bank1 (which is a problem).

I would have thought it would have remapped itself once the new code initialized, but that is not the case. Any suggestions would be appreciated. THanks