2012-06-28 04:41 AM
Hello,
I have been trying to programm the I-Flash while I am still working with interrupts. I can jump into the X-Flash and receive the data to programm. but when I start the programming process an error occurs, because an Interrupt comes and tries to read from the I-Flash (Interrupt array is in the I-Flash) How can I programm the I-Flash while still working with interrupts? I have tried using the SUSP bit from the Programming Flash resgisters. But it does not work. Thank you very much for all the help you can give to me! #programm-iflash #programm-st10