2005-05-02 07:35 PM
How does it work when negative volts is inputed on ST62T01C in assembly?
2005-05-01 07:47 PM
Hi everyone,
I have a big problem about negative input volts in assembly on MCU of ST62T01C. Normally, the data is 1111 1111(255 decimal) when positive input volts is 5V and also it is 0000 0000(0 decimal) when input volts is 0V. My question is that what digital value is when negative input volts is -2.5V. I am wating for your any answer immediately. Sincerely From Bob. :-[ [ This message was edited by: imbob on 02-05-2005 09:22 ]2005-05-01 09:04 PM
According to the absloute maximum ratings, you are not allowed a lower input voltage of -0,3V!
To measure -2,5V to +2,5V, you must add the input voltage with 2,5V. So -2,5V will be 0V! In the software the MSB is the negative flag! (one composite)2005-05-02 02:02 AM
Thanks a lot Moppie.
I cofirmed it that Vin is Vss-0.3V to Vss+0.3V on the datasheet of ST62T01C after your reply. However, could I get one more thing of it could be possible that Vss can be supplied negative volts? Thanks again. Regards. From Bob. :-D2005-05-02 07:35 PM
Yes it can, BUT don't forget the absolute maximum ratings!
The voltage between Vss and Vcc is 7V MAX. The input and output voltage are related to the Vss and Vcc. So it can, but take care!