cancel
Showing results for 
Search instead for 
Did you mean: 

Entering ICC mode with ST72F623 (ST72F623F2M1) ?

sooseokoh
Associate II
Posted on September 17, 2005 at 03:00

Entering ICC mode with ST72F623 (ST72F623F2M1) ?

5 REPLIES 5
sooseokoh
Associate II
Posted on September 09, 2005 at 02:00

Hi,

Does anyone know how to enter ICC mode with ST72F623 family?

I have tried to enter ICC mode in ''256 tcpu fixed window mode'', which is based on ICC protocol manual. But I couldn't enter ICC mode successfully. I have no idea now.

I used VPP pin for ICCSEL and sourced 4MHz frequency to OSC1 externally.

Properly sourced 38 pulses on ICCSEL pins (H2L) after RESET mode, which is that RESET goes high.

Maybe the period of 38 pulses are not short enough within 256 tCPU window under 4MHz external clock?

or Should I enter ICC mode through ''Controlled Windows mode''?

I tried this as well. Doesn't work either.

Am I missing something?

So .... I'm stuck now.

Please help me on this. :-[

Thanks!

sjo
Associate II
Posted on September 09, 2005 at 11:23

Are you writing your own programmer then, this is the only time you would need this info.

Have a look at the Flashbash source code where you will find an example of entering programming mode for this device.

look in the file icc.asm and the function ICCEnterFixed.

www.spen-soft.co.uk

Regards

sjo

sooseokoh
Associate II
Posted on September 16, 2005 at 04:05

Finally I was able to enter ICCMODE in 256 fxied window mode.!!!

Thanks a lot for the reply!!!

By the way,

Even thoguh I loaded my own flash programming code into RAM, I could not program HD flash.

I applied proper VPP of 12V voltage during program stage.

I'm just curious whether the device supports the Embedded Commands for HDFlash programming, which is an area of F8 ~ FF??

Does anyone know if the ST72F623F2 supports the HDFlash programming commands?

Thanks!

alok2
Associate II
Posted on September 16, 2005 at 04:32

See DFU examlpe f/w based on 7263 to take idea of HDflash prog

sooseokoh
Associate II
Posted on September 17, 2005 at 03:00

After little mistake at stack pointer for Embeded commands :)

I programmed the HDFlash successfuly !

Thanks a lot all of you guys! :-]