2005-06-16 10:08 PM
2005-06-16 02:07 AM
BOOTEN BOOT0 BOOT 1 MEMORY
0 X X FLASH (Internal) 1 0 0 FLASH (Internal) 1 1 0 RAM (Internal) 1 0 1 System-Memory 1 1 1 External Memory Bank 0(CS0 AREA : 0x60000000H) 1) When booting with boot option which is set 1 1 1 according to above, which is prior, CS0 signal or execution of StartupCODE? 2) In JTAGE DEBUGING MODE, should RAM(Internal) be set to 1 1 0? Now debugging is possible although composition of hardware is set to 1 1 1(External flash). 3) Must V18 Voltage be supplied from external? *** My Configreation CPU : STR710FZ ADS/AXD/MultiICE[ This message was edited by: Number2 on 16-06-2005 14:53 ]