cancel
Showing results for 
Search instead for 
Did you mean: 

unable to flash SPC560Bxx board

Santhamurthy R
Associate II
Posted on March 29, 2017 at 13:03

Hello All,

 I am using UDE 4.2 version for flashing SPC560B54L5 board.

When I am trying to Flash the program I am getting the error '' Failed to open FTDI driver'' as shown in the below snapshot. I also tried installing board specific FTDI driver (Royalty free d2xx direct driver for FT2232 part number) which is also not working.

0690X000006065WQAQ.png

kindly support in resolving the issue or kindly share the FTDI driver need to be installed

Thanks in Advance,

Regards,

R.Santhamurthy

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
?�ng Tr?n Thi�n
Associate II
Posted on March 30, 2017 at 09:37

Hi, first you check driver in Device Manager for see installation is successful? And it is recommended to use version 4.8 

If the driver is installed successfully, you try to check ''Config -> Target Interface...'' to see FTDI Device are display?

Wish you success

:)

 0690X00000606Y2QAI.png0690X00000606dJQAQ.png

Best regards

Dong Tran Thien

View solution in original post

2 REPLIES 2
?�ng Tr?n Thi�n
Associate II
Posted on March 30, 2017 at 09:37

Hi, first you check driver in Device Manager for see installation is successful? And it is recommended to use version 4.8 

If the driver is installed successfully, you try to check ''Config -> Target Interface...'' to see FTDI Device are display?

Wish you success

:)

 0690X00000606Y2QAI.png0690X00000606dJQAQ.png

Best regards

Dong Tran Thien

Erwan YVIN
ST Employee
Posted on March 30, 2017 at 09:48

Hello ,

if FTDI driver is not installed in your windows environment,

you can reinstall it,

the driver is located in this directory

c:\Program Files (x86)\pls\UDE Starterkit 4.8\JtagUsbDriver\

    Best Regards

                Erwan