2017-02-20 11:51 PM
Hello everyone, I'm working with SPC56EL60L3.
I'm doing some functional testing, and sometimes my application gest stuck.
This morning I found it stuck once again, I took a look using the debugger and I found it was exceuting _ivor_exit (please see the picture below)
Looking at the startup code (ivor.s), I found the following code, which looks like the only piece of code related to ivor_exit.
#if (CORE_SUPPORTS_DECREMENTER == 1)
/*
* _IVOR10 handler (Book-E decrementer). */ .align 4 .globl _IVOR10 .type _IVOR10, @function_IVOR10: /* Creation of the external stack frame (extctx structure).*/ e_stwu sp, -80(sp) /* Size of the extctx structure.*/e_stmvsrrw 8(sp) /* Saves PC, MSR. */
e_stmvsprw 16(sp) /* Saves CR, LR, CTR, XER. */ e_stmvgprw 32(sp) /* Saves GPR0, GPR3...GPR12. *//* Reset DIE bit in TSR register.*/
e_lis %r3, 0x0800 /* DIS bit mask. */ mtspr 336, %r3 /* TSR register. */#ifndef _SPC570Sxx_
/* Restoring pre-IRQ MSR register value.*/ mfSRR1 %r0/* No preemption, keeping EE disabled.*/
se_bclri %r0, 16 /* EE = bit 16. */ mtMSR %r0#endife_b _ivor_exit
#endif /* CORE_SUPPORTS_DECREMENTER */Reading the documentation I found IVOR_10 is related to decrementer interrupt.
As far as I understand, decrementer can be used for implementing software timing.
OK, what if I don't need decrementer (and I don't want its interrupt to interfere with my application?).
One more thing:
I found the following sentence on the programmers manual:
''MSR[EE] also enables external input and decrementer interrupts.'' (RM004, page 272)
It looks like whenever I enable interrupts setting the EE flag in MSR register (I use irqIsrEnable(), for this), it also enables decrementer interrupts.
What If I don't want decrementer interruotys to be enabled?
Should I make any changes to irqIsrEnable()?
Thank you.
Regards
Alessandro
2017-02-23 5:54 AM
Hello Alessandro ,
you should put this compilation switch in FALSE
#if (IRQ_ENABLE_IRQ_PREEMPTION == TRUE)�?�?�?
if you want disable IVOR10 (Decrementer),
youhave not to enable DIE (Decrementer Interrupt enable) in TCR SPR 340
asm (
'e_lis %r3, 0x0040 \t
' /* DIE ARE bits. */
'mtspr 340, %r3' /* TCR register. */
);�?�?�?�?
Best regards
Erwan