cancel
Showing results for 
Search instead for 
Did you mean: 

SPC58NN cannot debug after flash DCF

XJian.1
Associate

Debug tool:Lauterbach  Software Version: R.2018.02.000096069

The screenshot of CMM is as follows:

0693W00000NrSGtQAN.jpg0693W00000NrSGyQAN.jpgOf course, this cmm is modified by the cmm of the MPC5xxx chip

The above script writes two addresses,

0x00400360, the write data is 0x05AA55AF00000000

0x00400368, the write data is 0x0000030100080000 (start offline bist)

After executing the cmm, the debugger shows debug port fail.And the lower right corner of trace32 jumps reset from time to time

0693W00000NrSJYQA3.png0693W00000NrSJiQAN.png

I also learned about an official cmm from the "AN4939 How to run self-test in the SPC58NN84x device Rev2 March 2019.pdf" document, but I can't find this cmm on the official website, can you tell me where to download it?

0693W00000NrSKRQA3.jpg

So far, the above has happened to two boards, so desperately hope someone understands what happened and can let me know.

Best regards!

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

hello ,

your cmm file is relative to MPC5744P not SPC58NN

It is NXP application note.

i am checking with experts about SPC58NN cmm files.

Best regards

Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

hello ,

your cmm file is relative to MPC5744P not SPC58NN

It is NXP application note.

i am checking with experts about SPC58NN cmm files.

Best regards

Erwan