cancel
Showing results for 
Search instead for 
Did you mean: 

spc5 studio can't detect my board

TGecc
Associate

Good morning

We connected the board spc570 by microUSB, our operating system (both windows 7 and windows 10) detected it as "SPC570S-DISP discovery board" but can't install any driver. We have already downloaded and installed SPC5 studio with "complete installation" but it seems that it can't be aware of the connected device: we can generate application code and compile a test application but we can't execute and debug it because execute and debug button remains always grayed. So we will ask if we have to buy something else or we have to download some specific driver or change some setting on the PC.

best reguard

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee

Hello ,

it is not SPC5Studio .. it is linked to PLS UDE

PLS JTAG is integrated in your board

Could you check with PLS UDE 4.10 ?

https://www.pls-mc.com/login-a-384.html?User=SPC5UDESTKUser

You have to install it

  • SPC5Studio is a Development Environment
  • PLSD UDE is used to debug and flash your binary

Best regards

Erwan