cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5-MCTK-LIB_RTM_1_1_0_web, lack of #include "pal_lld.h"?

acarn
Associate

Hello,

there's problem when trying to build the project (Regardless which of the Web Motor Control Demos I choose).0690X00000ApTKCQA3.png

The steps I made are:

1.) Import samples from application

2.) Choose one of the motor control applications

3.) Generate the SPC5 Application

4.) Build the SPC5 Application

The last step generates following error message:

./components/spc56xx_web_motor_control_component/lib/System_Drive_Params/src/Spc5xxx_MC_it.c:48:21: fatal error: pal_lld.h: No such file or directory

 #include "pal_lld.h"

Which is a bit strange, since I didn't make any changes to the configuration.

Can you please help?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

1) MCTKLIB 1.1.0 is not compliant with SpcS5studio 5.8.1-Diadem

 There is Change Request to update the library .

2) MCTKLIB 1.1.0 is compliant with SPC5Studio 5.8.1 (Old Version)

http://mirrors.spc5studio.com/5.8.1/

you can use it without updated RLA components.

3) http://mctkcust.spc5studio.com is compliant with the last version but you need some credentials.

to be asked in credentials@spc5studio.com

Best Regards

Erwan

View solution in original post

5 REPLIES 5
Erwan YVIN
ST Employee

Hello ,

i think that the web site is not updated .

i have forwarded your request to the good person.

Best Regards

Erwan

Czhu.844
Associate

How about the problem? I also meet it ,help!

Erwan YVIN
ST Employee

hello ,

after the next release of SPC5Studio , we will post a new release located in web update site

Best regards

Erwan

Hello,

Was anything done about this ?

I have the same issue with SPC5-MCTK-LIB 1.1.0 and SPC5Studio 5.8.1 .

Erwan YVIN
ST Employee

Hello ,

1) MCTKLIB 1.1.0 is not compliant with SpcS5studio 5.8.1-Diadem

 There is Change Request to update the library .

2) MCTKLIB 1.1.0 is compliant with SPC5Studio 5.8.1 (Old Version)

http://mirrors.spc5studio.com/5.8.1/

you can use it without updated RLA components.

3) http://mctkcust.spc5studio.com is compliant with the last version but you need some credentials.

to be asked in credentials@spc5studio.com

Best Regards

Erwan