cancel
Showing results for 
Search instead for 
Did you mean: 

Need MCU with 2 CAN Transceiver and 2 Ethernet MAC

Mom.1
Associate II

Hi,

I need a MCU with 2 CAN transceiver and 2 EMAC interface for my design. I found that SPC58 series have the same. But the complete part number is not available from the site.

Please help me to find out the correct part number for design with 2 CAN transceiver and 2 EMAC.

Consider this as urgent and reply.

Warm regards,

Monisha OM

1 ACCEPTED SOLUTION

Accepted Solutions
zambrano.luigi
Senior III

Hi,

if your question is which MCU of the SPC58 family includes 2 CANs and 2 ETHs, the answer is the SPC58xG and the SPC58xH. Currently we have available also a development board (based on the SPC58xG), named SPC58NG-DISP, but it includes only one CAN transceiver.

Regards,

Luigi

View solution in original post

1 REPLY 1
zambrano.luigi
Senior III

Hi,

if your question is which MCU of the SPC58 family includes 2 CANs and 2 ETHs, the answer is the SPC58xG and the SPC58xH. Currently we have available also a development board (based on the SPC58xG), named SPC58NG-DISP, but it includes only one CAN transceiver.

Regards,

Luigi