2019-07-01 04:19 AM
.i need help with calculating clock and time peroid and waht is other pwm pin if pwm0 has d10 which is complemetary pin in spc56el70l5-disp
Solved! Go to Solution.
2019-12-13 03:24 AM
thanks for your help...i have one issue...my spc5660l5 is normally 40deg cel while it drive motor or CAN communication..is it normal..or am i drwing current from pwm pins...but spc5670 discovery though stays cool...as compared..is there an issue..
2019-12-22 11:57 PM
i need to know SPC56EL60L5 has EEPROM memeory...i have this driver component given in the example of SPC56EL70L5 but i change the platform..it shows error this device not supported by EED driver.whats is the isssue..please help.
2019-12-23 03:50 AM
Hi
currently the EEPROM Emulation Driver is provided only for the SPC56EL70L5 and not for the SPC56EL60L5.
Best Regards,
Luigi