cancel
Showing results for 
Search instead for 
Did you mean: 

How it is possible to program SPC582B60E1 MCU? Via JTAG, LIN-UART or CAN?

SBert.3
Associate

Hello,

I struggle to find precise information about SPC582B60E1 MCU programming.

With which interfaces it is possible to program it? JTAG, CANbus, LIN-UART?

Which kind of ISP is needed? Can I use a generic ISP that has jtag and UART interface?

Can you explain me the precise procedure to:

  • put the device in programming mode
  • flash the new firmware

Thank you in advice.

1 REPLY 1
Giuseppe DI-GIORE
ST Employee

JTAG: use UDESTK.