2014-07-10 05:34 AM
Hello,
I want to use canReceive and specify the mailbox to read (do not use CAN_ANY_MAILBOX). Example: if I want to check the first mailbox, I use:canReceive(can1.
canp
, 1, &rxmsg, TIME_IMMEDIATE) == MSG_OK canReceive first checks if the buffer received data using the can_lld_is_rx_nonempty function. If you give the mailbox number 1 to this function, it checks the mailbox 0 (BUF[0]). The problem is that next to this check, the function can_lld_receive will access the second mailbox (BUF[1]). To fix this, I suggest to define CAN_ANY_MAILBOX to 0xFF and change the switch values in can_lld_is_rx_nonempty from 1-8 to 0-7. My target is SPC56EL60 but it applies to all families and I use SPC5 Studio. Is it a bug or I missed something? I can't update SPC5 Studio at the moment, this bug is maybe already fixed. EDIT: using CAN_ANY_MAILBOX make these 2 functions searching through all mailboxes. In my example they both found that the first mailbox contains data, so it works... All the examples I found are using CAN_ANY_MAILBOX, did anybody tried to specify a mailbox number?2014-07-10 07:58 AM
mbid = mailbox-1;
}you can update manually :c:\SPC5Studio\eclipse\plugins\org.chibios.spc5.components.hal.platform.spc56elxx_1.0.0.xxxxxxxx\component\lib\src\can_lld.cthe correction will be available in the next updated version in spc5-hal component (can low level driver) Best Regards Erwan2014-07-16 06:01 AM
Hello,
it sounds logic to do so but it doesn't work. In debug on SPC56EL60 the functioncan_lld_is_rx_nonempty always returns false and I can't explain why! If I use CAN_ANY_MAILBOX it works... And I verified that each mailbox scans (for loops) were finding the mailbox number I passed (to replace CAN_ANY_MAILBOX).
And this solution doesn't allow to read the mailbox BUF[0] since CAN_ANY_MAILBOX is defined as 0... It's why I suggested to define it to 0xFF and change the switch cases 1-8 to 0-7 incan_lld_is_rx_nonempty.
Aurélien2014-07-16 09:04 AM
Hello Aurelien ,
1) When we transmit into MailboxID 1 .. in can_lld_is_rx_nonempty ... if canReceive (MailboxId=1), we are waiting for BUF[0]BUT The data is received in BUF[1].2) When we transmit into MailboxID 2 .. in can_lld_is_rx_nonempty ... if canReceive (MailboxId=2), we are waiting for BUF[1]BUT The data is received in BUF[1].your suggestion is good ;-)We are working on this issue and deliver a patch as soon as possible. Best regards Erwan2014-07-17 05:51 AM
Hello Aurélien ,
we can not set CAN_ANY_MAILBOX to 0xFF because this constant is used for others devices (STM32 and so on ..). in API level, the mailbox id should be between 1 and 8. the mailboxid for the reception depends on the EID used. our message has :txmsg.EID = 0x01234567; the CAN settings for OS-Less CAN application is (cf screenshot): Filter 0 Settings ==> Mailbox ID 1 (EID=0) Filter 1 Settings ==> Mailbox ID 2 (EID=0x01234567) Filter 2 Settings ==> Mailbox ID 3(EID=0) Filter 3 Settings ==> Mailbox ID 4 (EID=0) Filter 4 Settings ==> Mailbox ID 5 (EID=0) Filter 5 Settings ==> Mailbox ID 6 (EID=0) Filter 6 Settings ==> Mailbox ID 7 (EID=0) Filter 7 Settings ==> Mailbox ID 8 (EID=0) it means that if you transmit for a defined mailbox id : canTransmit(&CAND1, 1 to 8, &txmsg, TIME_IMMEDIATE) you should receive the message in mailbox id 2 (EID comparison) (cf Filter Settings): canReceive(can1.canp, 2, &rxmsg, TIME_IMMEDIATE) == MSG_OK the patch provided is working. It will be available in the official update site. i hope that i am clear. Best regards Erwan ________________ Attachments : 2014-07-17_144842.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWCb&d=%2Fa%2F0X0000000bo6%2FtBiD2ADDpYHHZ0TI3N2QHqCMzrb15BpXdaFTTe28fH8&asPdf=false2014-07-18 07:12 AM
#280836 can low level driver : Mailbox id issue in can_lld_receive
#266463
Add Chibios Components / Test Applications for SPC56ECxx family Best regards Erwan2014-07-22 02:19 AM
Hello Erwan,
I updated to org.chibios.spc5.components.hal.platform.spc56elxx_1.0.0.201407151616 and still it doesn't work when I use a mailbox number. In canReceive, the call ofcan_lld_receive is never reached. I configured mailboxes 1 to 3 and I successfully read their content when using CAN_ANY_MAILBOX. But when mentionning 1, 2 or 3, canReceive never return MSG_OK... I'm not in loopback mode. I send CAN frames using a PCAN interface.
Can anyone confirm that it works? Regards, Aurélien2014-07-22 02:41 AM
Hello Aurelien ,
By using the default configuration , and the patch, it is working well (cf Code Below) EID 0x1234567 while (TRUE) { /* * Sends the TX CAN Message. */ if (CANtransReq == 1) { if (canTransmit(&CAND1, 1, &txmsg, TIME_IMMEDIATE) != MSG_TIMEOUT) { palTogglePad(PORT_D, PD_LED2); CANtransReq = 0; } } /* * Receives the RX CAN Message. */ if (canReceive(can1.canp,2
, &rxmsg, TIME_IMMEDIATE) == MSG_OK) { /* Process message.*/ palTogglePad(PORT_D, can1.led); } } return 0; Write in BUF[1] (Cf Screenshot) Could you send me your application by email or forum ? Check your EID ''matching'' in Filter Settings ? Best Regards Erwan ________________ Attachments : 2014-07-22_114001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWUp&d=%2Fa%2F0X0000000boL%2FlL1cPFGXSMdi2tnGCmBYA0mvjjhoIHJ_qUJbfwFjh8s&asPdf=false