cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-IDB04A1 doesn't work

Andrey Semenov
Associate II
Posted on February 14, 2018 at 19:52

Hello,

I have an old board X-NUCLEO-IDB04A1 with BlueNRG chip and 32MHz HSO. Bulk ID: Z5T43269A018.

I implemented with it my own device based on STM32F407VGT6.

In firmware I setup minimun:

1. Execute ACI_GATT_INIT.

2. Execute ACI_GAP_INIT(Role=Peripheral)

3. Execute ACI_GAP_SET_DISCOVERABLE(Advertising_Type = 0x00, Advertising_Interval_Min = 0x0020, Advertising_Interval_Max = 0x0020, Own_Address_Type = 0x01, Advertising_Filter_Policy = 0x03)

This configuration you can see in AN4494 (Bringing up the BlueNRG and BlueNRG-MS devices).

Firmware stack is 6.3.

I turn on my device but laptop doesn't see it.

The firmware works because I watch Command Complete Events after execution of each command in debugger.

Tell me please, why factory manufactured board doesn't work? What should I do?

#bluenrg #x-nucleo-idb04a1
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0