Skip to main content
ismael teodoro
Associate II
February 12, 2018
Solved

LSM9DS1 magnetic interrupt don't work (is this a bug?)

  • February 12, 2018
  • 4 replies
  • 956 views
Posted on February 12, 2018 at 22:32

anybody helpe-me

LSM9DS1 magnetic interrupt

in my tests:

register INT_SRC_M no clear interrupt pin -> when read. (no away)

Does anyone have any ideas

?
This topic has been closed for replies.
Best answer by ismael teodoro
Posted on February 14, 2018 at 21:12

Hi everyone!!!

there is NO BUG no pin.

this pin only work with INT_THS_L(32h), INT_THS_H(33h) register.

I was wrong. I thought this pin had DRDY_M function.

my apologies

.

I'm sorry

:(

4 replies

Tesla DeLorean
Guru
February 12, 2018
Posted on February 12, 2018 at 23:17

Perhaps stick to one thread 

 

There's probably 5 or 6 registers that need setting up depending on what source(s) and threshold(s) you're attempting to use.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ismael teodoro
Associate II
February 13, 2018
Posted on February 13, 2018 at 14:15

thanks i put my config below

ismael teodoro
Associate II
February 13, 2018
Posted on February 13, 2018 at 14:14

Thanks for attention

this is my config test:

INT_GEN_CFG_XL(0x06) -> 0x00 //no interrupt accelerometer and gyroscope

INT1_CTRL (0x0C) -> 0x00 //no interrupt 1 accelerometer and gyroscope PIN

INT2_CTRL (0x0D) -> 0x00 //no interrupt 2 accelerometer and gyroscope PIN

CTRL_REG1_G (0x10) -> 0x00 //gyroscope POWER DOWN

CTRL_REG6_XL (0x20) -> 0x00//accelerometer POWER DOWN

INT_GEN_CFG_G (0X30) -> 0x00//no interrupt gyroscope

CTRL_REG1_M (0x20) -> 0x38//Magnetic Medium-performance mode 40Hz

CTRL_REG2_M (0x21) -> 0x20//Magnetic 8 gauss

CTRL_REG3_M (0x22) -> 0x00//Magnetic Continuous-conversion mode

CTRL_REG4_M (0x23) -> 0x04//Magnetic Z axis Medium-performance mode

INT_CFG_M (0x30) -> 0x85//Magnetic interrupt X axis, magnetic INT PIN enable, active high

after that the interrupt occur normally,

then i read INT_SRC_M (0x31) and magnetic interrupt pin no clear

Does anyone have any ideas

thanks

 
ismael teodoro
ismael teodoroAuthorBest answer
Associate II
February 14, 2018
Posted on February 14, 2018 at 21:12

Hi everyone!!!

there is NO BUG no pin.

this pin only work with INT_THS_L(32h), INT_THS_H(33h) register.

I was wrong. I thought this pin had DRDY_M function.

my apologies

.

I'm sorry

:(