cancel
Showing results for 
Search instead for 
Did you mean: 

Which MEMS microphone array(s) are compatible with the Omnidirectional microphone Nucleo expansion board?

DBrox.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @DB.7rox​ ,

there are basically two Nucleo expansion board that can be used in conjunction with all the ST MEMS microphones:

  1. X-NUCLEO-CCA02M2: X-Nucleo expansion board designed for the digital MP34DT06J mic, but can work with all the ST MEMS digital microphones (IMP34DT5A, MP23DB01HP, etc...)
  2. X-NUCLEO-AMICAM1: X-Nucleo expansion board designed for the analog MP23ABS1 mic.

Please let me know if I well understood your question.

-Eleon