2020-05-03 2:28 PM
My call back code looks like this:
char MotionMC_SaveCalInNVM(unsigned short int datasize, unsigned int *data)
{
// This function is called when a call to MothionMC_Initialize(sampletime,0) is made with
// data set to zero.
uint8_t i;
unsigned int *data_local;
data_local = data;
for(i = 0; i < datasize; i++)
{
otter_mag_cal_nvm[i] = *data_local;
data_local++;
}
return (char)0;
}...in debug, this code hard faults when the loop reaches 106. Far short of the st.com's MotionMC passed "datasize" of 184. The code has been tested to make sure the array otter_mag_cal_nvm[] is not at fault. For this testing the line "otter_mag_cal_nvm[0] = *data_local;" was used instead and the hard faults still occurred on the 106th iteration.
2020-05-04 12:25 AM
The datazise is number of bytes.
It is better to use memcpy command to copy data from the source to otter_mag_cal_nvm array. Please make sure the otter_mag_cal_nvm is big enough.
2020-06-15 12:45 PM
...
2020-06-15 12:45 PM
Hi @Miroslav BATEK ,
I have changed to using memcpy.
I am reading the calibration data provided when MotionMC calls back to the MotionMC_SaveCalInNVM() and used the IDE workspace Memory / Export feature to grab the compass calibration data and add it to a header file (our Nonvolatile Memory feature is not ready). Then, upon power up, I write the header file back into the structure provided by the call to the call back function MotionMC_LoadCalFromNVM().
But even after doing this my compass still requires the normal calibration maneuvers over the normal amount of time. So, I assume I am doing something wrong. I have read the compass calibration data several times and most values do are the same. Some values are different. But I assume this is because of subtle differences in how the compass was calibrated each time.
I was expecting the compass to report a 3 or "calibration good" immediately after the calibration data was written back. What might I be doing wrong?
-thanks
2020-06-26 9:17 AM
In fact unsigned int *data is bit misleading. The data is pointing to library internal data structure and should be saved/loaded as raw 184 bytes. Try to use:
#include <string.h>
...
uint8_t CalParams[184];
...
char MotionMC_LoadCalFromNVM(unsigned short int datasize, unsigned int *data)
{
memcpy(data, CalParams, datasize);
return 0;
}
char MotionMC_SaveCalInNVM(unsigned short int datasize, unsigned int *data)
{
memcpy(CalParams, data, datasize);
return 0;
}