2013-09-07 08:34 AM
What should I do with the 3 ADC input pins of the LIS3DH if not used?
#lis3dh #motion-sensor #accelerometer #accelerometer2013-09-09 09:26 AM
Hello Naue,
These 3 ADC input pins if not used can be tied to Vdd, or GND, or left floating. From a the power consumption point of view, it is recommended to tie them to either Vdd or GND. For more details, please check the attached detail sheet and visit Thank you, Thiago ReisFrom: naue
Posted: Saturday, September 07, 2013 5:34 PM Subject: What should I do with the 3 ADC input pins of the LIS3DH if not used? ________________ Attachments : LIS3DH.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzKg&d=%2Fa%2F0X0000000bJz%2FtH2q3.U0FmH_73bL0I2AeRlXVRf3wwti0hGbxD3QXiU&asPdf=false