cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum ODR selectable for the acquisition of signals for classification, understanding that the maximum ODR of the sensor is 6660 Hz ?

Evelina CAMILLERI
ST Employee
 
1 ACCEPTED SOLUTION

Accepted Solutions
Luca SEGHIZZI
Senior

Sensor ODR can be selected according to the specific application (up to 6.6 kHz). However, MLC is limited to four available data rates in ASM330LHHX: 12.5 Hz, 26 Hz, 52 Hz, 104 Hz. The data rate for MLC inputs is set through the MLC_ODR bits. If the sensor ODR is higher than MLC_ODR, MLC automatically decimates the input data (without any additional filtering).

It is recommended to select MLC_ODR equal to the sensor ODR to avoid decimation of the MLC inputs.

Selecting MLC_ODR lower than the sensor ODR is also possible, but the different frequency response could lower the accuracy of the MLC solution.

View solution in original post

1 REPLY 1
Luca SEGHIZZI
Senior

Sensor ODR can be selected according to the specific application (up to 6.6 kHz). However, MLC is limited to four available data rates in ASM330LHHX: 12.5 Hz, 26 Hz, 52 Hz, 104 Hz. The data rate for MLC inputs is set through the MLC_ODR bits. If the sensor ODR is higher than MLC_ODR, MLC automatically decimates the input data (without any additional filtering).

It is recommended to select MLC_ODR equal to the sensor ODR to avoid decimation of the MLC inputs.

Selecting MLC_ODR lower than the sensor ODR is also possible, but the different frequency response could lower the accuracy of the MLC solution.