cancel
Showing results for 
Search instead for 
Did you mean: 

What is the main difference between ASM330LHHX and LSM6DSOX? Which one is better?

Evelina CAMILLERI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Luca SEGHIZZI
Senior

LSM6DSOX and ASM330LHHX difference is that the first one is for consumer applications while the second is for automotive thanks to the AEC-Q100 compliancy. They both have the machine learning core and finite state machine feature embedded. Therefore, I can't tell which is better, you have to choose depending on the application you are targeting.

View solution in original post

1 REPLY 1
Luca SEGHIZZI
Senior

LSM6DSOX and ASM330LHHX difference is that the first one is for consumer applications while the second is for automotive thanks to the AEC-Q100 compliancy. They both have the machine learning core and finite state machine feature embedded. Therefore, I can't tell which is better, you have to choose depending on the application you are targeting.