cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L0X running on a 3.3 voltage rail

Tashfique
Associate II

We have designed a circuit using this chip with the 3.3 voltage rail . Without converting it to 2.8 as it is bellow the max thresh-hold as per the datasheet.

We also pulled up the XSHUT pin high to 3.3v using a 10k ohm resistor. In theory it should put the device into a software standby state. But the device doesn't turn on.

The only way we were able to turn on the device on was directly connecting the 3.3 v to the XSHUT pin, but it fails to do any sort of ranging.

We followed the Application schematic, described on the datasheet.

Any help will be greatly appreciated.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Aharon1
Associate II

any news on that issue?

Tashfique
Associate II

switched over to vl6180x and put a Voltage Regulator ...

Hardwariano
Associate III

We are using VL53L0X with 3.3 V rail and 10K pull-up resistors and it works. Perhaps its life span will be shortened.