cancel
Showing results for 
Search instead for 
Did you mean: 

Unico Lite GUI

daithi62
Associate II
Posted on May 16, 2017 at 18:23

Hi, is there any pdf available relating to the operation of the Unico Lite GUI. I have version 2.0.0.0 installed but I cannot seem to get it to communicate with the LSM6DS3.

Thanks

#lsm6ds3 #unico-lite
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Miroslav BATEK
ST Employee
Posted on May 17, 2017 at 15:30

I think Unico Lite GUI is quite obsolete SW. Don't you want to use rather the newest Unico 5.0 which you can find

http://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-mki109w.html

.

If you describe more what are you intention I can point you to the best SW and HW tools.

daithi62
Associate II
Posted on May 17, 2017 at 16:48

Thank you for the response Miroslav. The reason I downloaded version 2 was that it was on the downl;oad page for the STEVAL-MKI176V1. I have downloaded version 5 now. 

I am trying to communicate with the Gyroscope over SPI on the LSM6DS3 device on the 

STEVAL-MKI176V1 via  the STM32F103 microcontroller.

When I try to connect to the device using the GUI, I get the error attached. The firmware version isn't being recognised. The motherboard that I am using is a custom printed board. 

0690X0000060729QAA.png

Regards,

cod

Miroslav BATEK
ST Employee
Posted on May 18, 2017 at 13:53

Unico and Unico Lite are intended to work with eMotion board (

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mems-motion-sensor-eval-boards/steval-mki109v2.html

) or Professional MEMS tool (

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mems-motion-sensor-eval-boards/steval-mki109v3.html

).

You can connect all sensors available in DIL24 adapter like LSM6DS3 (

STEVAL-MKI176V1).

Please be aware you have to upgrate the firmware in the board by the one distributed together with Unico.

If you use your own board custom board you would have to write your own firmware compatible with Unico, which is very difficult.  

I would recommend you to send the data from your board only to terminal.