2025-10-20 4:10 PM
Hello,
I am using an LSM6DSV16X with an external sensor on Unico-GUI. I want to train a decision that uses both the internal and external sensors as inputs for the MLC. I am trying to save data from the internal sensors as well as the external sensors, but I do not find the option to include the external sensors in the "Load/Save" in Unico-GUI, even when the LSM6DSV16X is actively reading data from the external sensor through Unico-GUI's "Sensor Hub Registers" tab. How do I use Unico-GUI to save external sensor data, and if it isn't possible, how would I include external sensor data in the training for the MLC.
Thank you,
Abdurrahman Farag
Solved! Go to Solution.
2025-10-23 8:04 AM
Hi @Abdu ,
This feature is not currently available in Unico or MEMS Studio.
2025-10-23 8:04 AM
Hi @Abdu ,
This feature is not currently available in Unico or MEMS Studio.
2025-10-26 12:31 PM
Hello,
Thank you for your response. In the AN5804 document and LSM6DSV16X Datasheet, it mentions that MLC can use external sensor data as an input. How would I configure the LSM6DSV16X to include the external sensor data as an input? Would it require only that I include the sensor data in the training input? Please advise.
Thank you,
Abdurrahman Farag