2015-11-04 6:37 AM
I'm using the LPS25H pressure sensor and have noticed a strange stairstep behavior where one LPS25H seems to
step or jump 10-20 Pa for several minutes to a few hours, then jumps back. This behavior is quite differentfrom the normal RMS noise from sample to sample. I first noticed this when running several sensors sitting onthe same desk over a weekend using the other sensors as a reference. Note that step seems be some kind of fixedoffset since the relative pressure changes during the step does track with the other sensors.I have also see nthis behavior when doing a temperature sweep. In certain temperature bands the reading jumps out of the background atmospheric pressure trend, then snaps back when the temperature changes. In particularbelow 10C and a band around 20C.Is this behavior expected? I could expect some dift with temperature, but I would expect it to be more gradual.- Luke #lps25h2015-11-09 3:19 AM
Hello Luke,
0.1 to 0.2 mBar variations as in your description are expected from this class of devices, if you need better
performance from that point of view, I can suggest to use a newer generation of pressure sensors from ST such as LPS22HB.With Regards,
AdalbertoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.