2019-11-27 6:19 AM
In the document titled "STEVAL-MKI109V3 Professional MEMS Tool motherboard for MEMS adapter boards" UM2116, on p. 16 it is listed that the returned value from the *start command is: s t A_XH A_XL A_YH A_YL A_ZH A_ZL Int1 Int2 TL TH sw1|sw2 \r \n . This is incorrect as the device has a gyroscope and is returning 40 bytes. I need to know what these 40 bytes being returned actually are. Please advise. Thank you.