2020-11-10 4:12 AM
Hello,
I'm using STEVAL-STLKT01V1.
Then, I downloaded ST BlueNRG GUI 4.0.0, which provides these firmwares into the Firmware\BlueNRG_stack directory:
What is the best one to use?
If it is not one of these, or if a more updated version exists for it, where could I find the right one?
According to the documentation, the STEVAL-STLKT01V1 should be factory-flashed with bluenrg_7_1_e_Mode_2-32MHz-XO32K_4M.img, so in my opinion I should use bluenrg_7_3_Mode_2-32MHz-XO32K_4M.img but I prefer to ask to be sure before doing damages.
Thank you very much for your time.
Sincerely,
Carlo Bramini.
2020-12-02 8:58 AM
Hello,
>> You had the possibility to test the procedure on another SensorTile, right? And is it working on it?
Yes, it does (see last screenshot). I have not tried to do the download because I'm a bit worried to brick another one, but actually the *working* SensorTile is providing a different message when the "CONNECT" is done.
>> It's strange but yes, you could be right, especially in the case the FW is working on another SensorTile and not on your first one.
This is not a reassuring thing.
Sincerely.