2016-02-11 8:24 AM
Hi, I've tried to upgrade the firmware via DfuSe Demo, but it hung
After this, I've discovered that my STEVAL-MKI109V1 board has bricked.I can flash it again using a Nucleo Board's embedded STLink. I could test it and I've read the memory contents, so I am very confident about being able to write a binary on it.Is there someone who could send me a binary image for this board?PS: I've tried to extract .hex images from .dfu files inside ''stsw-mki109w.zip'', but all of them are bigger than 64kB (the size of STM32F102R8T6 that is on MKI109V1 board)2016-07-14 7:22 AM
Hello,
don't worry about size of hex file, it's size is many times higher than size of binary data. Try to program STEVAL-MKI109V1 with hex file you obtained from dfu file for example using ST-Link Utility.
Best Regards,
MarianWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.