cancel
Showing results for 
Search instead for 
Did you mean: 

STeval-MKI 109V1, also V2

fritzkendeffy
Associate II
Posted on December 29, 2011 at 11:04

Hi,

I intend to use several STeval-MKI109Vx structures, up to ten systems, simultaneously, and

all of them ''wireless''. STM offers a wireless Bluetooth kit for connecting to STeval-MKI109V1.

Is it possible to use up to 10 evalboards simult. with BT or would it be better to use ZigBee?

For example modules based on STM32W108xx.

Eventually these modules could be used without other uC, only by using the host W108xx

and adding a inertial sensor.

These should be ''streaming'' wireless nodes. 

thank's for answers
0 REPLIES 0