cancel
Showing results for 
Search instead for 
Did you mean: 

Sensor hub problems with LSM6DSV32X breakout, how to configure properly?

rbmarcus
Associate II

I'm trying to add an LIS2MDL (STEVAL-MKI181V1) magnetometer to my LSM6DSV32X's (STEVAL-MKI240KA) sensor hub. I can't get the LSM6DSV32X to properly identify the LIS2MDL, and I'm not sure if it's a hardware- or firmware-related problem. My current hardware configuration is:

  • SCx on MKI240KA tied to SCL on MKI181V1
  • SDx on MKI240KA tied to SDA on MKI181V1
  • INT2 on MKI240KA tied to DRDY on MKI181V1
  • Jumpers on MKI240KA shifted to SCx/SDx positions
  • CS on MKI181V1 tied to Vdd

For context I'm using Zephyr RTOS, but the initialization sequence for the LSM6DSV32X should be the same, especially since it fails right at the beginning when attempting to identify slaves. From the LA output, it looks like the LSM6DSV32X is trying to communicate with the external sensor but it can't sufficiently drive its SCx/SDx pins?

Screenshot from 2025-01-29 14-37-14.png

1 REPLY 1
Federica Bossi
ST Employee

Hi @rbmarcus ,

Your hardware configuration seems correct, but ensure that there are pull-up resistors on the I2C lines (SCL and SDA). Please refer to the section 7 of AN6016 where the sensor hub mode is well described:

FedericaBossi_0-1738251627758.png

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.