cancel
Showing results for 
Search instead for 
Did you mean: 

removing gravity from accelerometer reading

carl239955
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
S.Ma
Principal

We know the gravity vector size, not its direction.

AvaTar
Lead

If you can enforce a calibration (reference sampling at rest), and can keep track of movements (Nyquist !), you can subtract the gravity vecor out.

This is not possible within a singular point of time (one accelerometer sample), with unknown forces (accelerations) acting on it.

Eleon BORLINI
ST Employee

if you are not interested in measure uniform acceleration (but e.g. only harsh events), on most of ST accelerometers (let's say from LIS3DH family on), you can set an HP filter to remove the DC component from the 3-axis output signal, removing also the 1g gravity.

[in the other case, yes, you can remove the 1g value from the intensity of the 3-component vector, or referring to an initial known value/direction]

S.Ma
Principal

A kind of high pass filter with a certain response time...