2017-09-26 01:07 PM
I am using the code from STM32CubeFunctionPack_MOTENV1_V3.0.0 for sensor tile.
Initial I used the STlink to load the 'Projects\Multi\Applications\MOTENV1\Binary\STM32L476RG-SensorTile' MOTENV1_ST_BL.hex.
Then connect to the ST BlueMS.
When I trying out the 'Firmware upgrade' OTA feature in the Apps.
I select the 'MOTENV1_ST.bin' and copy it to the Phone.
Tried a few times of the OTA procedure and it always fail at the end 'Error sending the data'.
Is the binary file used on Phone for OTA correct ??
Regards,
Felix
2017-09-27 08:27 AM
OK, finally get FOTA working using my own build binary file. Somehow, the binary in release package always has error during send.