2019-09-02 6:57 PM
2019-09-10 3:20 AM
Hi @zjia.938nfeng , after a check with our experts they told me you could face some issue because this component has no entry for the FIFO in the filesystem. You can try the following steps:
1.Try to launch this function from the linux command line (checking if the interrupt pin of the magnetometer has been well connected to the processor):
generic_buffer -n lsm9ds1_accel -ga -c 10
generic_buffer -n lsm9ds1_gyro -ga -c 10
generic_buffer -n lsm9ds1_magn -ga -c 10
2.You could send us the Android logcat for our check
You could btw try to add this code to the SensorHAL and check if it's working:
diff --git a/src/SensorHAL.cpp b/src/SensorHAL.cpp
index 4df9553..5b95523 100644
--- a/src/SensorHAL.cpp
+++ b/src/SensorHAL.cpp
@@ -1171,6 +1177,9 @@ static int st_hal_load_iio_devices_data(STSensorHAL_iio_devices_data *data)
}
data[index].hw_fifo_len = device_iio_utils::get_hw_fifo_length(data[index].iio_sysfs_path);
+ if (data[index].hw_fifo_len <= 0)
+ data[index].hw_fifo_len = 1;
+
data[index].sensor_type = ST_sensors_supported[n].android_sensor_type;
data[index].dev_id = iio_devices[i].num;
diff --git a/src/utils.cpp b/src/utils.cpp
index 0075f2b..457f8f6 100644
--- a/src/utils.cpp
+++ b/src/utils.cpp
@@ -673,7 +672,19 @@ int device_iio_utils::set_hw_fifo_watermark(char *device_dir,
ret = snprintf(tmp_filaname, DEVICE_IIO_MAX_FILENAME_LEN,
"%s/%s", device_dir, device_iio_hw_fifo_watermark);
- return ret < 0 ? -ENOMEM : sysfs_write_int(tmp_filaname, watermark);
+ if (ret < 0)
+ return -ENOMEM;
+
+ ret = check_file(tmp_filaname);
+
+ if (!ret) {
+ ret = sysfs_write_int(tmp_filaname, watermark);
+ } else if (errno != ENOENT) {
+ /* permission error */
+ return ret;
+ }
+
+ return 0;
}If this still not work, please try this other code
diff --git a/src/utils.cpp b/src/utils.cpp
index 0075f2b..7ee7fb6 100644
--- a/src/utils.cpp
+++ b/src/utils.cpp
@@ -585,37 +584,37 @@ int device_iio_utils::get_hw_fifo_length(const char *device_dir)
ret = snprintf(tmp_filaname, DEVICE_IIO_MAX_FILENAME_LEN,
"%s/%s", device_dir, device_iio_hw_fifo_length);
if (ret < 0)
- return -ENOMEM;
+ return 0;
ret = sysfs_read_int(tmp_filaname, &len);
if (ret < 0 || len <= 0)
- return ret;
+ return 0;
/* write "len * 2" -> <iio:devicex>/buffer/length */
ret = snprintf(tmp_filaname, DEVICE_IIO_MAX_FILENAME_LEN,
"%s/%s", device_dir, device_iio_buffer_length);
if (ret < 0)
- return -ENOMEM;
+ return 0;
ret = sysfs_write_int(tmp_filaname, 2 * len);
if (ret < 0)
- return ret;
+ return 0;
/* write "1" -> <iio:devicex>/hwfifo_enabled */
ret = snprintf(tmp_filaname, DEVICE_IIO_MAX_FILENAME_LEN,
"%s/%s", device_dir, device_iio_hw_fifo_enabled);
if (ret < 0)
- return -ENOMEM;
+ return 0;
/* used for compatibility with old iio API */
ret = check_file(tmp_filaname);
if (ret < 0 && errno == ENOENT)
- return len;
+ return 0;
ret = sysfs_write_int(tmp_filaname, 1);
if (ret < 0) {
ALOGE("Failed to enable hw fifo: %s.", tmp_filaname);
- return ret;
+ return 0;
}
return len;Regards