cancel
Showing results for 
Search instead for 
Did you mean: 

LSM9DS1 Directional user orientation selection

Dmitrij Gendler
Associate II
Posted on March 08, 2018 at 17:11

Hi,

LSM9DS1 has the register ORIENT_CFG_G(13H).

What mean its bits     Orient[2:0]    Directional user orientation selection ?

Thanks

#directional-user-orientation-selection #lsm9ds1-directional-user-orientation-selection*
3 REPLIES 3
Miroslav BATEK
ST Employee
Posted on March 15, 2018 at 09:45

The bits Orient [2:0] in register ORIENT_CFG_G (0x13) can be used to change the axis orientation, as reported in following table.

0690X0000060A8EQAU.png
Dmitrij Gendler
Associate II
Posted on March 15, 2018 at 10:30

Thank you,

this table I've found in the datasheet for LSM6DS3US (September 2017  DocID028476 Rev 5).

As I use datasheet for LSM9DS1 (March 2015  DocID025715 Rev 3) the table is absent here.

There are some other reasons as well to ask: which release of datasheet for LSM9DS1 is the latest one?

Which others documents can be used for LSM9DS1 may be with some notes (e.g. I’ve seen an explanation of self-test for LSM9DS1 on base of a document for another chip).

Posted on March 15, 2018 at 16:56

The datasheet DocID025715 Rev 3 from March 2015 is the latest one.

Yes, the table is missing there, it should be fixed soon.

There is no other document for LSM9DS1.