2024-09-27 09:20 AM
Hi,
I am looking at the LSM6DSO device, and I am unclear what the "USR_OFF_ON_WU" bit does in the "WAKE_UP_THS " register. Does this bit:
Can someone please provide clarity?
thanks
2024-10-09 07:17 AM
Hi @Dude ,
When it is set to '1' the input data for the wake-up function comes from the low-pass filter path (instead of the high pass filtered data) and the programmable position is subtracted as an offset.