cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO FIFO Timestamp Gets Reset After 0xFFFF

BDiva.1
Associate II

Any ideas on why the timestamp gets reset in FIFO after 0xFFFF? I have TIMESTAMP_EN bit of the

CTRL10_C register set to 1 and the DEC_TS_BATCH_[1:0] bits of the FIFO_CTRL4 are set to 01 (max(BDR_XL[Hz],BDR_GY[Hz]) [Hz]).

1 REPLY 1
niccolò
ST Employee

Hi @BDiva.1​ ,

there are two reason for which the timestamp can reset:

you wrote that it resets after 0xFFFF, but what register are you reading? is it TIMESTAMP 0 and 1, or 2 and 3?

Niccolò