2016-02-25 10:26 AM
Greetings.
I am trying to get accurate gyro data out of the LSM6DS3, but my results are about 15% off of what I expect.
My test setup is a PASCO scientific Rotary Motion Sensor (RMS) with a LSM6DS3 mounted on top of it.
I configured the LSM6DS3 such that full scale +/-32767 is mapped to +/- 1000 dps.
I then rotated the RMS and LSM6DS3 at 366 dps (as measured from the RMS) and the LSM6DS3 gyro reported a z-axis rotational value of 10173.My calculated gyro z-axis rotational velocity for this value is
10173 counts * (1000 dps / 32767 counts) = 310 dps.Why is the gyro reporting 310 dps when it is being rotated at 366 dps?
What is the guaranteed accuracy of the gyro?Thank you
Scott Wild2016-03-17 7:19 AM