cancel
Showing results for 
Search instead for 
Did you mean: 

LPS22HH temperature readings

hmckee
Associate

Anyone have any idea if the temperature can remain the same for long periods of time in a stable environment?

2 REPLIES 2
Federica Bossi
ST Employee

Hi @hmckee ,

It should. Did you try?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Yes, that's the issue. We've set up our device so that it marks the LPS22 in error if it reads the same value 45 times in a 30 min period. The condition has occurred in both a stable, temperature controlled environment and in an uncontrolled environment.

The purpose of this was to determine if the LPS22 is functioning properly. Maybe this is an unrealistic expectation.