cancel
Showing results for 
Search instead for 
Did you mean: 

LPS22HB gives inconsistent readings

DGand.2
Associate

Please refer this thread. I don't think that the sensor can get damaged in such short period of time. Is it possibly due to moisture? At times I get 1018hPa which is even higher than sea level pressure of 1013.5 hPa

Pls help.

1 REPLY 1
Federica Bossi
ST Employee

Hi @DGand.2​ ,

Welcome to ST Community!

On pressure sensors there are very small holes on the silicon exposed cap area of the package to allow external pressure to reach the sensing element and for this reason they should be kept clear of obstructions, in particular humidity can affect the measures.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.