cancel
Showing results for 
Search instead for 
Did you mean: 

log data conversion

joseph_binu
Visitor

Hello guys,

I am using the STEVAL-MKPRO BOX, i want to use MLC with this box. For that i tried to log data(Accelerometer data) with BLE Sensor application. The data is stored inside the micro SD . I connected the SD card to my computer and saw that  it was a .dat file. I tried to convert it into a format which is compatible with ST Mems studio with stdatalog_to_unico.py in the stdatalog-pysdk but it is not working  .I also tried using the nb_stdatalog_converters.ipynb under how_to_notebooks section but literally only the cell with conversion to unico was not working, all the other cells were working. What can i do ?

Thank you in advance

Screenshot 2025-10-10 154312.png

Screenshot 2025-10-10 150847.png

0 REPLIES 0