cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3MDL single measurement mode

Guillaume Reinhardt
Associate II
Posted on June 12, 2017 at 12:08

Hello, 

I would like to use the LIS3MDL magnetometer in single measurement mode to reduce my overall current consumption.

I've found some useful informations in the AN4602 Application but I'm still missing something.

The turn on time, from wakeup command to data availability, is specified (as a function of the operating mode) but 

the current consumption during turn on is not given.

What value should I use for my calculations?

Thanks

Guillaume

#power #lis3mdl
2 REPLIES 2
Petr S
ST Employee
Posted on September 04, 2017 at 13:18

Hello 

Guillaume,

I've asked the sensor specialists to get you an answer. Please hold on, if you don't have a chance to measure it directly on your HW setup.

Regards,

Petr

Petr S
ST Employee
Posted on September 05, 2017 at 12:04

Hello 

Guillaume,

In single measurement mode, for ODR < 10 Hz, the average current consumption can be calculated with the following formula:

(Current_consumption_10Hz - Current_consumption_in_power_down) / (10 Hz / ODR) + Current_consumption_in_power_down

Regards,

Petr