2016-07-20 06:35 AM
The LIS3DSH was implemented into one of our systems and currently we are having an issue with the Temperature readings across multiple units in the same environment vary from one another up to 15ºC.
Is there a way to calibrate the temperature on the LIS3DSH, or is it not recommended to use?The reason we are tracking temperature with it, over a temperature range the values change as described in the datasheet. And during our calibration process we are taking multiple temperature readings and normalizing the variance. Is it possible to ''reset'' the temperature in a controlled environment, or is this something where we would have to use a software offset? Also, those that show a large swing between actual temperature and readings, does this cause any adverse effects to the accelerometer measurements?2016-08-12 12:23 AM
The temperature sensor can be used to measure temperature variations. It isn't suitable to return absolute temperatures measures. The value represents difference respect to a reference not specified value.
Is not possible modify the temperature offset of the sensor by the user.
The different temperature offset between devices does not impact the devices performances.
Best regards
Miroslav