Skip to main content
Paul Mellor
Associate II
January 23, 2017
Question

LIS3DSH at +- 24g

  • January 23, 2017
  • 1 reply
  • 4244 views
Posted on January 23, 2017 at 18:13

The spec for the LIS3DSH quotes +-16g, yet the sensitivity at full scale is 0.73mg/LSB, giving a full scale range of +-24g. Can the sensor be used effectively at +-24g? What kind of non-linearities or other errors might arise at these higher levels?

This topic has been closed for replies.

1 reply

ST Employee
January 24, 2017
Posted on January 24, 2017 at 11:51

Hello Paul,

ST doesn't guarantee any parameters above +-16g. The senor will measure something, but it wont be linear and it can vary sensor by sensor.