2014-04-13 2:10 AM
Hello Community,
I am encountering a problem while debug single and double click function on the LIS3DH. 1. If the LIS3DH is configure for single click event detection, the single click interrupt is generated when a single input stimulus. 2. If the LIS3DH is configure for single and double click event detection, only the double click interrupt is generated when a double input stimulus, the single click interrupt never generated when a single input stimulus. What causes it, I am very worried. I would appreciate any help, thank you in advance! #lis3dh