cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH - Power Consumption

BToft
Associate II

Dear Forum. 

I use a LIS3DH connected with a Pic mainboard. I cummunicate with I2C and have set it up with interupt. I use 8mg, Lowpower and 50 hz odr. 

I have a problems with Power Consumption. Before i insert the LIS3DH it use 3 microampere. After i have set it up with interupt i use 100 microampere. We use a STEVAL-MKI105V1 eval board. 

How can i set it up so it only use 10 micro ampere. 

 

 

 

Best regards

 

Bjarne 

Profort. 

4 REPLIES 4
Federica Bossi
ST Employee

Hi @BToft ,

That's sound strange LIS3DH in LP mode and ODR 50Hz should have a power consumption of 6uA. Can you share your schematic?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
BToft
Associate II

I have here a diagram. It is a testmodule. 

combispot.jpg

Hi @BToft ,

Can you try to connect also SDO and CS according to the datasheet?

FedericaBossi_0-1720605088230.png

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.