2013-10-04 7:39 AM
Hello,
I'm hoping to get a bit of guidance here on this application I'm developing using the LIS331HH device. I have integrated it into the application PCB, and using SPI to communicate with the device. All is well and I can set and read registers, ODR, filters, range, etc. Also, for actual implementation, I have tied the 2 HW interrupt lines to the microcontroller and will be using that in future. For the time, I just want to understand how to implement the right code to deliver the desired outcome. Using some test code, I can see data coming from xL, XH, yL, yH, zL, ZH but don't fully realize how to apply it for the desired outcome. The application is very straightforward; to measure forces on the PCB that are primarily in 1 axis. After looking at a handful of code samples (there are few to be found) it's gained some clarity but still not there. Also, I didn't find the app notes helpful in terms of actual code implementation. I understand that the orientation of the device is quite relevant to the data output. The PCB when installed in the assembly can ''roll'' (in x-y) about the Z-axis (meaning Z axis is horizontal relative to me) So exactly what do I need to do with the output data to meaningfully use it? Here are some questions I hope someone can answer for me: 1 - The range of the device is +/-24g. Can I extend this to just +48g? How? 2 - How do I ''normalize'' the actual position relative to the absolute (calibrated) position and apply this to the data of interest? 3 - I'm primarily interested in the Z force vector. I also understand that there may be relevant applicable forces from x,y contributing to z, as the device rolls about on the z axis. Can I use the simple square root of sum-of-squares to tabulate total force on Z? I would be mostly appreciative of a code sample, algorithm or clear explanation for this objective. Thank you, regards, Gary #lis3312013-10-22 6:11 AM
Hello Gay,
Please check the answers to your questions below:1 - The range of the device is +/-24g. Can I extend this to just +48g? How?
- This is not possible the maximum FS available in this accelerometer is +/- 24g. 2 - How do I ''normalize'' the actual position relative to the absolute (calibrated) position and apply this to the data of interest? - I am not sure what you meant by normalize, but you can set up an average to determine your product initial's positioning, and then develop your solution based on that reference. 3 - I'm primarily interested in the Z force vector. I also understand that there may be relevant applicable forces from x,y contributing to z, as the device rolls about on the z axis. Can I use the simple square root of sum-of-squares to tabulate total force on Z? - I believe the Z-axis of the accelerometer already gives you a good idea of what is going on with the z-forces, that is because the sensor computes each axis indenpendetly, so, if you tilt your product, then, the x - y and z values will show a variation due to that movement. ST does offer a tool for evaluation that can help you on your development, the Unico plataform that you can find on the link below:http://www.st.com/web/en/catalog/tools/PF257815
Please do let me know if there is anything else that I can do to support you? Thank you very much, ThiagoHello,
I'm hoping to get a bit of guidance here on this application I'm developing using the LIS331HH device. I have integrated it into the application PCB, and using SPI to communicate with the device. All is well and I can set and read registers, ODR, filters, range, etc. Also, for actual implementation, I have tied the 2 HW interrupt lines to the microcontroller and will be using that in future. For the time, I just want to understand how to implement the right code to deliver the desired outcome. Using some test code, I can see data coming from xL, XH, yL, yH, zL, ZH but don't fully realize how to apply it for the desired outcome. The application is very straightforward; to measure forces on the PCB that are primarily in 1 axis. After looking at a handful of code samples (there are few to be found) it's gained some clarity but still not there. Also, I didn't find the app notes helpful in terms of actual code implementation. I understand that the orientation of the device is quite relevant to the data output. The PCB when installed in the assembly can ''roll'' (in x-y) about the Z-axis (meaning Z axis is horizontal relative to me) So exactly what do I need to do with the output data to meaningfully use it? Here are some questions I hope someone can answer for me: 1 - The range of the device is +/-24g. Can I extend this to just +48g? How? 2 - How do I ''normalize'' the actual position relative to the absolute (calibrated) position and apply this to the data of interest? 3 - I'm primarily interested in the Z force vector. I also understand that there may be relevant applicable forces from x,y contributing to z, as the device rolls about on the z axis. Can I use the simple square root of sum-of-squares to tabulate total force on Z? I would be mostly appreciative of a code sample, algorithm or clear explanation for this objective. Thank you, regards, Gary2013-10-22 11:35 AM
2013-11-18 4:24 AM
Hello Gary,
In order to provide a better feedback to you, could you please send me a screenshot of the issue that you are facing? The evaluation board should be working with the installed application. Thank you very much, Thiago Reis2014-12-18 12:20 PM
Hello Reis,
I am currently working with LIS331HH sensor and able to read the X,Y,Z registers. However, these values are in data type int16. How can I convert it to acceleration in engineering units ? Does the range -32768 to 32767 correspond to -12g to 12g respectively ? My FS1 & FS0 are 0 and 1 Respectively.Please advise.Thanks,Kamal Joshi